2021-01-11 2:51 AM
Hi, I use a X-NUCLEO-BNRG2A1 with a NUCLEO-L476RG .
My goal is to describe a card reader (USB CCID class) with the HID service. I tested my HID service with the report map of a mouse and it works I can make it move.
Now I send the USB descriptors of the CCID class to the report map. Is it possible to describe a USB class in the report map?
2021-01-11 10:31 PM
Possibly not,
as CCID descriptor is seen in the interface descriptor indicating Smart Card Class code, and not in the report descriptors.
2021-01-15 5:39 AM
@Winfred LU Thank you for the answer, indeed it does not seem to work.
Is there a way to change the HID service interface descriptor to create a ccid class in BLE? Or can we create or use a BLE service that will add the CCID class?