cancel
Showing results for 
Search instead for 
Did you mean: 

BLE : Cannot enable notification on the client characteristic configuration descriptor (0x2902)

malarab
Senior II

Hello,

i defined a characteristic with notify propriety : 

 ret = aci_gatt_add_char(
Service2_Handle1,
UUID_TYPE_128,
&char_uuid,
26,
CHAR_PROP_NOTIFY | CHAR_PROP_WRITE | CHAR_PROP_WRITE_WITHOUT_RESP,
ATTR_PERMISSION_NONE,
GATT_NOTIFY_ATTRIBUTE_WRITE | GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP,
16,
1,
&Service2_Char_Notify_Handle);

with CHAR_PROP_NOTIFY  it is generate  CCCD and by default Client Notification is disabled.

I need to enable it on the server, so i tryed with this code :

 Service2_Char_Notify_NotifDesc_Handle = Service2_Char_Notify_Handle+2;
ret = aci_gatt_set_access_permission(
Service2_Handle1,
Service2_Char_Notify_NotifDesc_Handle,
(0x01 | 0x02)); //Access_Permissions

uint8_t char_notify_ennotifdesc_val[2] = {0x01,0x00};
ret = aci_gatt_write_char_desc(connection_handle, Service2_Char_Notify_NotifDesc_Handle, 2, char_notify_ennotifdesc_val);

 But in debugging with an android app, the notification will stil disabled !

 

How can i enable the notification to the client from the server ?

 

Thank you, 

Sincerely.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

it is ok, i resolved the problem with aci_gatt_set_desc_value

it is look like  aci_gatt_write_char_desc is specific for cilent side,

but aci_gatt_set_desc_value work on the server side

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @malarab 

I think this link may give some help.

Best regards.

II

it is ok, i resolved the problem with aci_gatt_set_desc_value

it is look like  aci_gatt_write_char_desc is specific for cilent side,

but aci_gatt_set_desc_value work on the server side