2017-04-19 12:41 PM
I have a SPWF01 with last firmware 3.5 (160129). But i am facing a problem with setup of the time (AT+S.SETTIME).
Each time i send the command the module does not answer and make reset after 20 seconds, i send the command the module accept it.
I want to setup the time to make a one-way authentication.
Do you know what is wrong?
Solved! Go to Solution.
2017-04-19 02:19 PM
Hi,
there is an issue on the very first SETTIME command after poweron. A watchdog reset. It was already fixed, and will be part of next FW release.
There are no issues after hw reset, or sw reset. Only when RTC is cleared (remove power supply).
Best regards
jerry
2017-04-19 02:19 PM
Hi,
there is an issue on the very first SETTIME command after poweron. A watchdog reset. It was already fixed, and will be part of next FW release.
There are no issues after hw reset, or sw reset. Only when RTC is cleared (remove power supply).
Best regards
jerry
2017-04-20 11:50 AM
Thanks Gerardo,
I made a reset CFUN=1 at the begging at it works.
This is a serius issue ST must write it on the manual and release new firmware.