cancel
Showing results for 
Search instead for 
Did you mean: 

Are the SPSGRFC-868 and SPSGRFC-915 Spirit1 radio modules physically different? Since the antenna for these modules is separate, is there a need for physically different modules?

PVilb.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @PVilb.1​, to the community!

the SPSGRFC-868 and SPSGRFC-915 are identical in terms of board and dimensions, only the balun and carrier frequencies are different. Of course, the antenna used must match the module used, i.e. 433/868/915MHz.

Does it answer your questions?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

Welcome, @PVilb.1​, to the community!

the SPSGRFC-868 and SPSGRFC-915 are identical in terms of board and dimensions, only the balun and carrier frequencies are different. Of course, the antenna used must match the module used, i.e. 433/868/915MHz.

Does it answer your questions?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you Peter. We were hoping that the modules wouldn't be physically different from PCA inventory management, but since the balun is different we will have to forecast, build and inventory separate North American and European PCAs.

Best,

Patrick Vilbrandt

[... phone number removed ...]

OK!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Peter,

I have a follow-up question for you.

For FCC certification, the TAOGLASS TI.19.2113 antenna that the SPSGRFC-915 module lists as the required antenna is ridiculously long (over 15") for use with our products (one which is 4 3/4" x 2 3/4" x 1 1/2"). We would like to use something like the LINX ANT-915-CW-QW, which is very similar to the antenna listed with this module for CE certification.

Has ST done a modular certification, or is ST considering certification with a similar more reasonable length antenna?

Thanks again,

Patrick Vilbrandt

[... phone number removed ...]

It is mandatory to comply with the radiation limits, and ST has only carried out the certification with selected, named antennas. Of course, other antennas can also be used, in which case the unit must of course undergo the corresponding certification. Details on the FCC certification process can be found in AN5566.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

BTW: please do not reply with your e-mail client, because it usually includes contact details (telephone number, etc), which is then visible worldwide here in the public forum.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.