cancel
Showing results for 
Search instead for 
Did you mean: 

aci_gatt_update_char_value fails

milind2
Associate II
Posted on January 07, 2017 at 08:54

The function aci_gatt_update_char_value fails initially....and if fails there is while(1) loop...so system stuck here....what is issue ? after debugging it observed that function returns BLE_STATUS_TIMEOUT.....can you suggest solution for issue

6 REPLIES 6
Oliver Beirne
Senior
Posted on January 09, 2017 at 10:50

Hello

We have forums setup to ask questions which you can see from the forums menu at the top of this page. Which ST product are you working with?

Thanks

Posted on January 09, 2017 at 10:55

We are using Bluetooth module BlueNRG-MS

Posted on January 09, 2017 at 12:23

INTERFACE AND CONNECTIVITY ICS

Posted on January 09, 2017 at 12:39

I have moved this thread to

https://community.st.com/community/interface-and-connectivity-ics?sr=search&ampsearchId=a98a5b89-7b79-4a61-acda-25eddf4d6774&ampsearchIndex=0

.  

,

or

Gallucci.Gerardo

can you help with this question or tag someone who could?

Thanks

Antonio Vilei
Senior III
Posted on January 10, 2017 at 12:05

I replied to this question here:

https://community.st.com/0D50X00009XkeiRSAR