Skip to main content
NKohl.1
Associate II
November 25, 2021
Question

X-Nucleo 53L5A1 works fine with Windows GUI, but does not even init / is not alive using API

  • November 25, 2021
  • 11 replies
  • 3155 views

Hello,

the VL53L5CX is a really nice senor. I have done some measurements using the Windows GUI and was impressed, so I wanted to write a driver for the sensor and do some further evaluation.

I then tried to initialize the sensor using the ULD-API and my Nucleo-Board, but the sensor is not detected via I²C, I double checked with the Windows GUI - everything works just fine - so the Hardware should be alright.

I tried using the provided example in the API - same problem. I did not do anything fancy yet, are there some known issues? What is the Firmware in the Windows GUI doing different than the API? The init() loads the default firmware to the sensor, how long does that take?

Background:

  • I am using the latest API V1.1.2
  • I am using the platform.h and .c from the example
  • I²C address is VL53L5CX_DEFAULT_I2C_ADDRESS
  • before calling init() I set GPIOs PWR_EN_C, LPn_C, and reset I2C_RST_C
  • I make sure to wait long enough for the power supply to be stable

What else could go wrong?

Thank You for Your help!

Kind regards,

Niklas

This topic has been closed for replies.

11 replies

NKohl.1
NKohl.1Author
Associate II
December 7, 2021

The STM32F401 and the STM32L476 are both little endian. The function you mentioned is not included in the API, there is a SwapBuffer in platform.h, and vl53l5cx_dci_read_data, vl53l5cx_dci_write_data, and vl53l5cx_dci_replace_data in the api.

I changed the byte order, which resulted in the sensor not initializing, because the endianess should have been wrong when reversing the byte order, since the F401 and the L476 have the same endianess.

Changing the byte order would also not affect the value of the target status, which is a uint8_t.