cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-TOF1 dependencies

DMeie.2
Senior II

The Release Notes for the X-CUBE-TOF1 Library mention as dependencies

  • STM32CubeHAL F4 V1.7.12
  • STM32CubeHAL L4 V1.13.0

Where can I get these HAL libraries?

My STM32Cube Package Manager is currently set to use the STM32F4 MCU Package 1.26.2.

What about CPUs other than F4 and L4? Will the X-CUBE-TOF1 Library not work with those?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

The ToF sensors don't care what MCU is being used. All the hardware cares about is the I2C bus.

(non-ST MCUs work too - but don't tell anyone.)

Unfortunately I don't actually know if the X-CUBE-TOF libraries work with the others, but I cannot imagine why not. Those are very generic C code. So although I don't have proof, I'm betting they do.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.