Skip to main content
Associate
April 18, 2024
Solved

vl53l0x sensor detection distance inquiry

  • April 18, 2024
  • 3 replies
  • 1796 views

(A translator was used for this inquiry.)

Hi,

I am using the vl53l0x sensor.
I would like to inquire about the detection range of the sensor.

  1. What value do you get when the wall you want to measure the distance against is tilted? (Refer to image1)
    What point distance do you get if the minimum length between the sensor and the wall is 100 mm and the maximum is 200 mm?
  2. I know that the maximum measurement distance of the sensor is 2M.
    I would like to know the range of the detectable area when the wall and the sensor are 2M away.
    (Refer to image2)

Thank you.

This topic has been closed for replies.
Best answer by John E KVAM

The cone of light - or it' Field of View is 27 degrees. 

With a little trig one sees that the diameter of the illumination circle is 1/2 the distance. 

The astute reader will do the math and get 0.44 but it's a question of accuracy. 

Very near the sensor the FoV is wider, and it narrows as the distance increases.

So, go with 1/2 and you will be as good as you are going to get.

- john

3 replies

John E KVAM
ST Employee
April 18, 2024

In the first image when you have a slanted wall, you will get the average of all photon return times.

The trouble is that near objects return more photons than a far object. So instead of the mathematical average, you will see a number weighted toward the closer distance. 

Unfortunately, how much of this effect you see will depend on the reflectivity of the wall.

 

As far as a wall at 2M what you get will depend on the reflectivity of the wall. If it's bright enough to return photons you will get 2M and status =0. A less reflective will will give you Staus =2 (low signal). With a REALLY bright target, beyond 4M you will get a status 4. Status 4 means you have a wrap around issue. Wrap-around (also called Aliasing) is a condition where the photons from pulse A get returned after the pulse of pulse A+1. So with a bright wall beyond 4M, you get a Range Status =4 and the correct distance minus the 2M wrap around point. 

If this bothers you, a pin-compatible part (VL53L3CX) is available. It's an L0 part with better mathematics.  

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
pcbsmtAuthor
Associate
April 19, 2024

Thank you for your kind reply.

Regarding question 2, I am curious about the detectable area.

The sensor's detection range appears to be gradually expanding in a cone shape.
Then, I would like to know the area of ​​the detectable area from a distance of 2M.
(Part marked with a question mark in Image 2)

 

Thank you.

John E KVAM
John E KVAMBest answer
ST Employee
April 19, 2024

The cone of light - or it' Field of View is 27 degrees. 

With a little trig one sees that the diameter of the illumination circle is 1/2 the distance. 

The astute reader will do the math and get 0.44 but it's a question of accuracy. 

Very near the sensor the FoV is wider, and it narrows as the distance increases.

So, go with 1/2 and you will be as good as you are going to get.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.