cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 VL53L7CX SMART PRESENCE DETECTION

Arun28
Associate

Hii,

I am working on a project using the STM32 Smart Presence Detection. In order to run the program and get the detection for the person and get some detection readings which file and what are the steps should I follow? I have extracted the STSW-IM048 file and I have played with the EVK interface and now I am struggling to use this algorithm to implement this system to my robot.

1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

Once you have played with the graphical User Interface (GUI) in the presence code (STSW-IMG048) you want to try programming. 

Find the .zip file and unzip it. 

navigate to: C:\...\VL53L5_PresenceHODKit_1.0.82\Projects\Multi\Applications\VL53L5\PresenceHODKit\STM32CubeIDE\STM32F401RE-Nucleo\

(Don't worry about the L5 above. Same as L7, but with a wider Field of View. And yours might not be 1.0.82)

At this point you are going to want to have STM32CubeIDE installed on your computer. It's free. Download it from ST.com

Get STM32CubeIDE open, select "file", 'open project from file system' and give it the directory name where you see the .cprogect file. IC:\...\VL53L5_PresenceHODKit_1.0.82\Projects\Multi\Applications\VL53L5\PresenceHODKit\STM32CubeIDE\STM32F401RE-Nucleo

From here you should be able to compile and run. Then try debugging the program and see what it is doing. 

Get that going and you will be up to speed. There is a compiled library that does the presence stuff. 

C:\...\VL53L5_PresenceHODKit_1.0.82\Middlewares\ST\PresenceDetect\HODMZ

You can bring that library to other machines and compilers. But if it's not an ARM processor you are going to need some support. (In this case open a support ticket and I will support you.)

- john

 


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

3 REPLIES 3
John E KVAM
ST Employee

Once you have played with the graphical User Interface (GUI) in the presence code (STSW-IMG048) you want to try programming. 

Find the .zip file and unzip it. 

navigate to: C:\...\VL53L5_PresenceHODKit_1.0.82\Projects\Multi\Applications\VL53L5\PresenceHODKit\STM32CubeIDE\STM32F401RE-Nucleo\

(Don't worry about the L5 above. Same as L7, but with a wider Field of View. And yours might not be 1.0.82)

At this point you are going to want to have STM32CubeIDE installed on your computer. It's free. Download it from ST.com

Get STM32CubeIDE open, select "file", 'open project from file system' and give it the directory name where you see the .cprogect file. IC:\...\VL53L5_PresenceHODKit_1.0.82\Projects\Multi\Applications\VL53L5\PresenceHODKit\STM32CubeIDE\STM32F401RE-Nucleo

From here you should be able to compile and run. Then try debugging the program and see what it is doing. 

Get that going and you will be up to speed. There is a compiled library that does the presence stuff. 

C:\...\VL53L5_PresenceHODKit_1.0.82\Middlewares\ST\PresenceDetect\HODMZ

You can bring that library to other machines and compilers. But if it's not an ARM processor you are going to need some support. (In this case open a support ticket and I will support you.)

- john

 


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

I could not find any files like this C:\...\VL53L5_PresenceHODKit_1.0.82\Projects\Multi\Applications\VL53L5\PresenceHODKit\STM32CubeIDE\STM32F401RE-Nucleo\

John E KVAM
ST Employee

My fault for not checking the latest. I just downloaded it and saw version 1.0.0

Go to:

STSW-IMG048\SPD_kit_1.0.1\

SmartPresenceDetectionKit_F401_1.0.0\SmartPresenceDetectionKit\STM32CubeIDE\STM32F401RE-Nucleo\

This directory has the .cproject file in it. 

Some guy decided to clean it up for the initial release to customers. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.