cancel
Showing results for 
Search instead for 
Did you mean: 

Can this product VL53L0X work in high vaccum range condition( 10^-3 to 10^-8 torr)? What is the resolution of this product VL53L0X? What is working temperature range of this product VL53L0X?

YM.2
Associate

Can this product VL53L0X work in high vaccum range condition( 10^-3 to 10^-8 torr)?

What is the resolution of this product VL53L0X?

What is working temperature range of this product VL53L0X?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

The sensor has air in it. But there is a hole - otherwise it would explode during reflow. But the datasheet says a slow ramp up is required to allow time for the air pressure to escape.

So the vacuum is not the problem but a rapid change in air pressure would be.

The resolution is 1mm. However the accuracy is more like +/- 3%. And maybe +/- a 5mm below 2cm.

The working temperature is stated in the datasheet - -20 to +70 degrees C.

If you need higher temps and better short distance linearity, just wait. It's almost out.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

2 REPLIES 2
John E KVAM
ST Employee

The sensor has air in it. But there is a hole - otherwise it would explode during reflow. But the datasheet says a slow ramp up is required to allow time for the air pressure to escape.

So the vacuum is not the problem but a rapid change in air pressure would be.

The resolution is 1mm. However the accuracy is more like +/- 3%. And maybe +/- a 5mm below 2cm.

The working temperature is stated in the datasheet - -20 to +70 degrees C.

If you need higher temps and better short distance linearity, just wait. It's almost out.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
YM.2
Associate

Thank you @John E KVAM​