cancel
Showing results for 
Search instead for 
Did you mean: 

Are the registers and addresses same for VL6180V1 and VL6180X?

RGura.1096
Associate II

I would like to use VL6180V1 in one of my project.

I am interfacing it with STM8L MCU. For the sake of simplicity, I would like to copy the settings of the arduino library of VL6180X :

 https://github.com/sparkfun/SparkFun_ToF_Range_Finder-VL6180_Arduino_Library

and

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00122600.pdf

I would like to know if it would work or not because of the difference between VL6180 and VL6180X (Presence and absence of ALS). If not, then please guide me with the register setup.

The API that is available is for STM32 and not STM8. Hence I am requesting for this clarification.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
John E KVAM
ST Employee

The silicon inside the VL6180V1 and VL6180X are indentical. No changes are needed.

Have no fear. If you don't need the ALS going from the X part to the V1 part will take no work on your part.

And you will save a few cents.

(We don't have to buy the ALS filter and we don't have to calibrate the ALS. So we can sell the part to you for a few cents savings.)

I did have one customer that went from the no-ALS to the ALS and he had trouble until he covered the ALS opening. (Which is exactly what we did when we invented the V1 part.) But you won't have this issue.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
RGura.1096
Associate II

Great. Thanks for the reply John.