Question
NMEA 230400 baud rate with Teseo-Suite Pro 6.1.3.0
Hi,
I am using the suite with a TeseoIII set to output at 230400 baud rate.
When in this rate the suite does not auto-detect it and does not connect automatically as it does in 115200.
When configured manually to this rate, it can communicate and show the signal level, but in this rate it cannot open the skyview, the Firmware wizards cannot start and the firmware configuration panel cannot start.
Do you have a newer tool version that is capable to resolve the above?
Thanks.