| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, I am starting to learn and use Bluenrg-2 BCN002-V1 and tried to flash it using the example...
| 2024-10-15 4:17 PM | ||
|
Hi We are currently working on a design involving the TSV912IQ2T operational amplifier for piezo f...
| 2024-10-15 10:45 AM | ||
|
Hi, I am using X-NUCLEO-BNRG2A1 mounted on NUCLEO-STM32L496. I want to implement security so I am u...
| 2024-10-10 10:00 PM | ||
|
Hi, Trying to compile one of the BlueNRG-LPS example project in Keil. And get the following err...
| 2024-10-10 9:53 AM | ||
|
In the Spirit1 driver code, two registers at address 0x99 and 0x9A are being written. These don't ...
| 2024-10-08 9:30 AM | ||
|
Hi,
I'm debugging a board with two STMP34 used to read voltage and current from L1 - L2 and L3 of...
| 2024-09-20 6:56 AM | ||
|
Has anyone in the community used the ST7540 PLM in an airport environment ? I am working on a FAA...
| 2024-09-04 1:44 PM | ||
|
Hi,
I'm currently learning how to create an IO-LINK device using the NUCLEO-G071RB and X-NUCLEO-I...
| 2024-09-02 1:52 AM | ||
|
Hi., Good after noon., we are using LBEE5HY1MW-230 and WSM-BL241-ADA-008 wife+BLE module for O...
| 2024-09-02 12:09 AM | ||
|
Hi, Is there any information regarding whether there are internal clamping diodes to VDD and GND o...
| 2024-08-26 3:11 AM | ||
|
What is the simplest way to set the power amplifier? Unfortunately the APIs require involvement wi...
| 2024-08-19 10:46 AM | ||
|
I am trying to receive calls when a device receives scan requests but I can not get the events to ...
| 2024-08-15 6:13 AM | ||
|
Hi, I am working on a project that involves, among other things, BLE communication. The host side o...
| 2024-08-12 10:52 AM | ||
|
What is the current into VSYS when reset is high and VDD is 0V?
| 2024-08-09 8:22 AM | ||
|
We have a problem to drive a crystal some of the PCB on after the mass production as we tought h...
| 2024-08-08 11:36 PM | ||
|
Background: I have implemented an IO-Link communication slave device using IO-Link PHY chi...
| 2024-08-06 6:18 PM | ||
|
Hello,
I am experiencing issues with my STEVAL-IDP004V2 evaluation board. When I connect the devi...
| 2024-08-04 10:59 AM | ||
|
Hello to STM community,
I am sharing my problem with you regarding STEVAL-IHP005V1 evaluation kit...
| 2024-08-01 10:36 PM | ||
|
Hi, I am testing the STEVAL-BFA001V2B development kit to evaluate the use of the IOLink protocol. ...
| 2024-07-31 12:41 AM | ||
|
ST BLE Sensor 5.2.4 is closed once "Blue Voice Full Duplex" is selected.
Below error message show...
| 2024-07-30 12:46 AM |