| Subject | Author | Posted | |
|---|---|---|---|
|
Hello,
We are evaluating Bluetooth capability to our system using ST Bluetooth module, in order t...
| 2025-01-22 2:26 AM | ||
|
I’m testing S2-LP sub-GHz transceivers in stack packet mode. I’m encountering an issue where the se...
| 2025-01-21 10:17 PM | ||
|
I am using this code to read the RMS Voltage and Current. I am also able to get output which I have...
| 2025-01-15 5:27 AM | ||
|
Hello, Following AN4872 & UM2667 I did the following: - Connected J15(Force DIO7 High). - UAR...
| 2025-01-09 6:28 AM | ||
|
My team is trying to design a radio board with the STM32WL and we plan to use the BALF-WL-00D3 i...
| 2025-01-07 8:13 AM | ||
|
Hello ST Community, I am working on a project that involves implementing the STUSB1602 to act as a...
| 2024-12-15 2:56 PM | ||
|
Hello everyone,
I am experiencing a voltage issue between the IO-Link master and IO-Link devi...
| 2024-11-25 2:45 AM | ||
|
Hello all, I have a B-L475E-IOT01A2 Discovery Kit board and need to send 250kpbs rate of data from...
| 2024-11-14 5:46 AM | ||
|
I'm trying to perform a remote firmware update, with the bluenrg-lp ota service manager, I reco...
| 2024-11-13 10:13 AM | ||
|
Hi,
I am trying to connect the STEVAL-BFA001V2B to a siemens ET-200SP IO-Link master. I have flas...
| 2024-11-13 7:11 AM | ||
|
Hello all,
I'm trying to send 160 2-byte samples through the BLE platform each 10ms ( total bitra...
| 2024-11-12 1:35 AM | ||
|
I want to build a gateway that supports BLE and subGHZ frequencies (433 and 915MHz). Is it possible...
| 2024-11-12 1:22 AM | ||
|
Hello everyone, I bought an X-Nucleo-BNRG2AI board for a project I need to do using Bluetooth. I c...
| 2024-11-02 11:32 AM | ||
|
I am doing g3-PLC test by connecting two board of EVLKST8500GH-2
according to ST G3-Hybrid PLC&R...
| 2024-10-28 8:07 AM | ||
|
Could someone help to understand the better value to use at frequency deviation, considering at bel...
| 2024-10-23 10:24 AM | ||
|
Hi
I am developing RF transceiver with S2-LPQTR, frequency range 413-479 MHz. Also I bought BALF-...
| 2024-10-23 5:34 AM | ||
|
I want to use this configuration according to the L9663 Datasheet "Trigger via SPI with an upstream...
| 2024-10-22 11:06 PM | ||
|
Hello, maybe you have an idea!?! The STEVAL-IHP005V1 is connected to a 12V power supply and a seri...
| 2024-10-22 1:25 AM | ||
|
Hello everyone, I’m seeking guidance on using the STEVAL-USBI2CFT as a voltage shifter (to 3.3V) a...
| 2024-10-21 10:56 AM | ||
|
Hallo, So I have this ADV_IND advertisement mode, which works just fine: // Advertisi...
| 2024-10-18 5:25 AM |