Subject | Author | Posted | |
---|---|---|---|
My project consists of two STM32WB A master and a slave. The master will run the p2pRrouter example...
| 2020-02-19 12:32 AM | ||
I have a Raspberry Pi and an NCP running as the OpenThread Border Router. The thread commissioning ...
| 2020-02-18 08:06 AM | ||
I have managed to build the STM32WB Zigbee example applications using Atollic TrueStudio after some...
| 2020-02-13 07:01 AM | ||
I have a struct defined as: struct sendIP_struct {
char node_type[12];
char description[8];
ui...
| 2020-02-12 10:09 PM | ||
Hi, i am trying to get familiar with stm32wb55 BLE functionality. As a part of it, i tried with H...
| 2020-02-12 09:20 PM | ||
When generating project with BLE "Utilities" folder is marked "Exclude resource from build" but it ...
| 2020-02-12 05:10 AM | ||
Hello there. I have been trying to send some data over BLE, but am facing some challenges. When ...
| 2020-02-11 11:27 PM | ||
I use B-L072Z-LRWAN1 LoRa®/Sigfox modul, to make communication over sigfox. I made prototype with m...
| 2020-02-05 06:04 AM | ||
Hi, I am trying to get familiar with stm32cubemx usage. For this, i want to update an existing gpio...
| 2020-02-05 01:08 AM | ||
Waiting an app note like F0xx family. Could someone post routines for Page Erase and double Progra...
| 2020-02-04 12:58 PM | ||
Hello, I have some problem with running ble mesh on other device than nucleo. Someone tried run ...
| 2020-01-31 03:32 AM | ||
Hey there, bringing my custom STM32WB board up, I encountered a problem with the RTC initializat...
| 2020-01-29 02:27 AM | ||
Hi, I'm testing the STM32CubeFunctionPack_BVLINKWB1_V1.1.0 package. is it possible to stream audio ...
| 2020-01-27 11:59 AM | ||
Hi, I am using the STM32L0 LoRa Discovery kit and trying to upgrade the firmware via USB DHU. I ha...
| 2020-01-24 05:20 AM | ||
Does STM32WB chip comes pre-programmed with DFU bootloader from factory? If not where I can find ...
| 2020-01-17 07:25 AM | ||
I want to use the OpenThread UDP API. So far I implemented the UDP datagram reception without any p...
| 2020-01-14 02:16 AM | ||
We are currently working on STM32WBCC. Let's say my device name is DEVA. Have the following questio...
| 2020-01-10 03:58 PM | ||
2020-01-09 01:49 AM | |||
I am currently working on STM32CubeExpansion_LRWAN_V1.3.1 projects. I am using STM32l073 mcu. In ...
| 2020-01-07 07:01 AM | ||
Stack versions: LRWAN_V1.3.0, LRWAN_V1.2.3, LRWAN_V1.2.2 Hardware: B-L072Z Murata module We are...
| 2020-01-03 10:03 AM |