cancel
Showing results for 
Search instead for 
Did you mean: 

The spurious emojis are back

Andrew Neil
Super User

example, viewing the posted message:

AndrewNeil_0-1745408308978.png

 

https://community.st.com/t5/stm32-mcus-embedded-software/explanation-about-flash-memory-on-sector-method/m-p/795729/highlight/true#M62609

 

But wile editing that message:

AndrewNeil_1-1745408347682.png

 

But OK again after posting:

AndrewNeil_2-1745408420276.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
3 REPLIES 3
Andrew Neil
Super User

Oh, it's worse than that!

As you can see, the colon and closing parenthesis are in the wrong order in the posted comment:

AndrewNeil_0-1745408585523.png

So I go to edit it, and put them in the correct order:

AndrewNeil_1-1745408645565.png

But when I post, they get transposed again:

AndrewNeil_2-1745408695020.png

So the forum has converted it to the text form of an emoticon, but then not rendered it as an emoji graphic!

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Seems to work OK on an initial reply:

AndrewNeil_1-1745414423262.png

AndrewNeil_2-1745414448544.png

https://community.st.com/t5/power-management/stpm01-ic-offset-values-at-zero-voltage/td-p/795844

 

So just on editing a reply?

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Lina_DABASINSKAITE
Community manager

Hi @Andrew Neil , 

Thanks for reporting. I can confirm the behavior during the edit action on my side. 

We have a bug registered when emoji interferes with text and code elements which is currently in the fix phase. We are expecting the fix to be done in a couple of weeks.

Once it's completed, we will see if this behavior is fixed too. Will keep you posted on the results.

Apologies for the insolvencies in the meantime. 

BR,
Lina
 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.