cancel
Showing results for 
Search instead for 
Did you mean: 

Replies are being eaten?

TDK
Super User

I am 100% sure I replied to this thread:

https://community.st.com/t5/stm32-mcu-products/do-not-use-hal-spi-transmit-for-high-performance-dma-may-not-be/m-p/570578#M217483

As evidence, I am "subscribed" to it and get notified of new posts, which happens only if you reply, or if you click the subscribe button which I never do.

TDK_0-1687983495834.png

However, when I go to that page, I don't see my contribution anywhere in that thread. Am I missing something? Do replies get eaten occasionally?

@waclawek.jan Any ideas or similar experiences?

If you feel a post has answered your question, please click "Accept as Solution".
1 ACCEPTED SOLUTION

Accepted Solutions
Amelie ACKERMANN
Community manager

Hello @TDK,

Thanks for reporting this to us. Unfortunately, your reply was marked by the automated spam prevention mechanism and had to be unlocked first. It is now visible and part of the discussion thread. Please apologize this hurdle. We will further refine the automated spam prevention to avoid similar cases in the future.

Best,
Amelie

 

View solution in original post

18 REPLIES 18

I've been logged out automatically when creating a post, and it errors when I try to submit. Swear I've had to copy the content so I don't lose it.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Amelie ACKERMANN
Community manager

Hello @TDK,

Thanks for reporting this to us. Unfortunately, your reply was marked by the automated spam prevention mechanism and had to be unlocked first. It is now visible and part of the discussion thread. Please apologize this hurdle. We will further refine the automated spam prevention to avoid similar cases in the future.

Best,
Amelie

 

waclawek.jan
Super User

> Any ideas or similar experiences?

Maybe?

I am constantly trying to figure out which the threads I was answering recently are, and together with fighting the automatic reload in FF just to be able to make a couple of posts it takes up so much of my energy, that if some of my replies got lost I probably wouldn't even notice at this point.

[deleted lengthy rant, trying to be positive]

There is some sort of autosave, but I am not sure upon what stimulus does it save. I've been offered surprising chunks of half-written posts in the past.

JW

waclawek.jan
Super User

This post?

waclawekjan_0-1688024551299.png

I attest I haven't seen it there yesterday, even when reading KnarfB's reply to my post.

Also, @KnarfB would most probably reply to it or mention it, would he've seen it there yesterday.

JW

JW

Hello @Tesla DeLorean,

Sorry to hear this! In order to report to IT, can you share further details? 

  • Does the automated logout happen every time and on different browsers?
  • Does it happen when posting a reply as well as when posting a new question?
  • Do you get any error notifications?

Thanks, 
Amelie

Yes, @waclawek.jan I can confirm that I didn't see @TDK s reply before yours and my reply.

KnarfB

waclawek.jan
Super User

Oh c'mon, do you (and all ST) really need to be told AGAIN that LOGIN TIMEOUTS as such ARE BAD, BAD, BAD?

JW

waclawek.jan
Super User

Okay, so thanks to this thread being replied recently, I was able to remember one case when my reply got lost: I posted there a test, just putting there those two filenames, and that just disappeared, without any notification.

To be sure, I now repeated the test, here's the proof of post:

waclawekjan_0-1688026851974.png

with my offending post at the end, and this is how the thread looks after reload:

waclawekjan_1-1688026998008.png

So, what I guess happened with TDK's post is, that it got automatically censored; and then somebody manually restored it after TDK complained here.

JW

Okay, that would explain the situation. I don't see what in my post would look like spam. Several sentences long, no links.

It's frustrating when a contribution just disappears like that, with no notification even to me. I'm left here questioning my sanity.

If you feel a post has answered your question, please click "Accept as Solution".