cancel
Showing results for 
Search instead for 
Did you mean: 

"Latest reply" stats are sometimes incorrect

TDK
Super User

Clicking on a user's name to view their profile, I can see their previous posts. For example:

TDK_1-1756326161630.png

It says the last reply to the thread was a week ago. However, when viewing that thread, there are 4 more replies after mine. The latest reply should reflect the last such reply.

 

How widespread is this problem? 2/4 of the posts from this user show a "latest reply" which is not the latest.

 

I viewed a few other user profiles and could find the same problem happening. Probably 25% or so are wrong. Here are a few:

TDK_2-1756326510752.png

TDK_3-1756326605411.png

 

If you feel a post has answered your question, please click "Accept as Solution".
1 REPLY 1
Lina_DABASINSKAITE
Community manager

Hi @TDK,

Thanks for bringing this up!

To replicate this:

  • I checked now the profile of: About PKurz.1
  • But I see a different output then you. @TDK.

Lina_DABASINSKAITE_0-1756380378765.png

Questions:

  • Did you capture your screenshot on August 27, 2025, or earlier?
  • To define the urgency of this matter, can you share how often do you/or anyone else, use this component and for what use case?

I’ve raised this topic with our vendor to see if there are any issues with this component.
I will get back once I have news.  

Regards,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.