cancel
Showing results for 
Search instead for 
Did you mean: 

How to verify email address ?

debugging
Lead

On some post now I get an error

debugging_0-1771125006604.png

Have been on this forum for 8 years or so, never had this issue..

I tried to report a fix to someone, can't do that.. This is a great way to block uses reporting solutions.

What is this ? Cannot find any link how to verify.

Please help ASAP

I also don't see Sidekick on any forum, is that related ?

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @debugging,

The team has implemented the necessary changes for the second point. The text that appears when hovering over the chatbot now states: Open STM32 Sidekick.

 
 

Screenshot 2026-03-04 133645.png

Thank you for highlighting this point. 
Lina 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
TDK
Super User

> On some post

The post is likely read only, as the message suggests. Perhaps provide a link. You're clearly able to interact with the forum by making this post.

If you feel a post has answered your question, please click "Accept as Solution".
Lina_DABASINSKAITE
Community manager

Hi @debugging

To confirm what @TDK said. This text appears for read-only threads, and you are logged out. If it's not the case, please send over a screenshot and URL where it does appear to you. 

As for the Sidekick, it's working and should appear on Welcome page and on all STM32 MCUs and STM32 MPUs related forum boards. Share a screenshot where it does not appear to you. 

Regards,
Lina 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
debugging
Lead

thanks for the reply.

1. Yes I was logged in and Yes the thread was locked/read only.  I was  wondering i needed to verify  my email address or how I could see my email is "verified" or not and there wasn't a verify option in my profile. As I was logged in perhaps the error message could be more intelligent.

2. I understand now that "sidekick" is the icon. when I moved my mouse over the icon it said "open chat" . I could not find the word "sidekick" in any of the webpages so wondered what or where it was.

debugging_0-1771507270847.png

3.  I am not sure why I see the icon it now. perhaps related to https://community.st.com/t5/feedback-forum/having-issue-with-stm32-sidekick-with-firefox/m-p/865804  but I use Ubuntu with Firefox.

 

 

 

Hi @debugging

Thanks for additional information. 

For the 1st point - I am checking if the notification message can vary based on the log-in status. If not, we will have to keep it as it is. 

For 2nd - I have passed the feedback to the respective team. I will let you now once there are news on this. 

Regards,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@debugging wrote:

I could not find the word "sidekick" in any of the webpages so wondered what or where it was.


In Developer News: STM32 Sidekick: the AI-powered tool that accelerates your design journey.

In the Knowledge base: How to use STM32 Sidekick.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Lina_DABASINSKAITE wrote:

I am checking if the notification message can vary based on the log-in status.


It seems to be the standard message - example screenshots here and here.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi @debugging,

The team has implemented the necessary changes for the second point. The text that appears when hovering over the chatbot now states: Open STM32 Sidekick.

 
 

Screenshot 2026-03-04 133645.png

Thank you for highlighting this point. 
Lina 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.