cancel
Showing results for 
Search instead for 
Did you mean: 

Code blocks are too long

Piranha
Chief II

https://community.st.com/t5/stm32-mcus-products/uart-receive-issue/m-p/602914/highlight/true#M226105

How am I supposed to view a code at a longer lines, which have to be scrolled to the right, if the horizontal scrollbar is 8 screens down? And such a long blocks are not usable anyway. There is a simple solution for both of these issues - limit the maximum vertical size of the code blocks. The size should definitely be smaller than the average screen size. Probably some 30-40 visible lines of code are fine.

2 REPLIES 2
Lina_DABASINSKAITE
Community manager

Hi Piranha, 

Thanks for the feedback provided! I will check what options to we have to adjust to the requirements and get back to you. 

Thanks a lot, 
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Piranha
Chief II

https://community.st.com/t5/stm32-mcus-products/can-dma-trigger-mdma-block-transfer-linked-list/td-p/603854

Even a better example - select a superlong post as a solution and you get two superlong posts... :face_with_tears_of_joy: