2023-10-30 06:54 PM - edited 2023-10-31 06:56 PM
https://community.st.com/t5/stm32-mcus-products/uart-receive-issue/m-p/602914/highlight/true#M226105
How am I supposed to view a code at a longer lines, which have to be scrolled to the right, if the horizontal scrollbar is 8 screens down? And such a long blocks are not usable anyway. There is a simple solution for both of these issues - limit the maximum vertical size of the code blocks. The size should definitely be smaller than the average screen size. Probably some 30-40 visible lines of code are fine.
2023-11-03 04:08 AM
Hi Piranha,
Thanks for the feedback provided! I will check what options to we have to adjust to the requirements and get back to you.
Thanks a lot,
Lina
2023-11-09 04:16 PM
Even a better example - select a superlong post as a solution and you get two superlong posts...