cancel
Showing results for 
Search instead for 
Did you mean: 

Is the ESDCAN compatible with FlexRay?

LauraCx
ST Employee

Is the ESDCAN compatible with FlexRay?

Yes, it is compatible with Flexray for ESDCAN02 and 03. And even more, as the line capacitance is lower than 3.5 pF it will be compatible with the next generation of CAN like CANXL.

Comments
hshay.1
Associate

very good and simplified explanation, strictly point wise.

Version history
Last update:
‎2022-09-15 08:37 AM
Updated by: