cancel
Showing results for 
Search instead for 
Did you mean: 

Using STM32H745 with Model zoo - Computer vision - AI

syalam
Associate

I want to run Cube AI Model zoo examples on STM32H745. The current example in Model zoo is for STM32H747 with a display, I can replace the display and print the output on UART. 

 

Is there an example or tutorial that explains the changes required to run AI on STM32H745? I would appreciate a detailed answer with a guide, as I am new to STM MCUs.

 

Development kits: NUCLEO-144 STM32H745ZI EVAL BRD

1 REPLY 1
Julien CLOSS
ST Employee

Hello,

As of today, the application examples contained in the STM32 Model Zoo are supporting only two STM32 boards:

- The STM32H747 DK board, and

- The STM32H743 Nucleo board.

Thank you.

Julien.