2023-07-01 12:37 AM
Hello! Im using STM32Cube IDE version 1.12.1.Im having isssue with including the header file "ai_platform.h " and "ai_datatypes_defines.h".I have installed X-cube-AI extensions and all other required extension of Artificial Intelligence.I am getting the error message of "no such file or directory" .I request you to look into the issue.
Thank you !
2023-07-01 9:29 AM
look, are this "missing" files in path ? maybe, you have to add path... if not there.
2023-07-02 10:09 PM
Where can I find these missing files ?Middlewares files are missing in project file.I downloaded the STM32 Cube IDE on 28th of June 2023. Is there any further update ?
2023-07-03 12:25 AM
no, you misunderstood.
if download was ok, all needed files should be there.
just maybe , a path to use/include is wrong or missing; that i wanna show.
so first take an example project, to see, all is working.
and for missing .h -> search file on your disk, then control, that this is in path-settings (or add, if not there)