Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST seeks data scientists: Participate in a paid usability session

Hello ST Community members,   Are you a data scientist or machine learning engineer with experience deploying neural networks on edge or embedded devices? The ST team invites you to join a 45-minute remote usability session to provide technical feedb...

camera not working properly

im trying to run a model that distuingish pasta types using stm32h747i and camera . i followed this guide  https://wiki.stmicroelectronics.cn/stm32mcu/index.php?title=AI:How_to_use_Teachable_Machine_to_create_an_image_classification_application_on_ST...

20240727_140125.jpg
yessine by Associate III
  • 721 Views
  • 1 replies
  • 0 kudos

Used Ram over External SDRAM and TFlite Micro runtime

It seems like a used ram size fit to External SDRAM in STM32H757i- EVAL Board.However, I can see the error when doing analyze.Also, I cannot see any TFLite Micro runtime generated code.I can see empty function.I was totally fine with STM32CUBE AI run...

pepsi_zero_sugar_1-1724297824905.png pepsi_zero_sugar_0-1724297679218.png pepsi_zero_sugar_2-1724297847147.png pepsi_zero_sugar_3-1724297983155.png

Resolved! Class in the output of the refernece model

When I used validation app I could see like  notes: - the output of the reference model is used as ground truth/reference value         - 10 samples (5 items per sample)   acc=100.00%, rmse=0.000000147, mae=0.000000066, l2r=0.000000430, nse=1.000, co...

pepsi_zero_sugar_0-1724124147197.png

modelzoo unrealibility

I wanted to share some feedback regarding the use of ModelZoo, as you previously recommended. Unfortunately, after dedicating significant time—about a month—to working with it, I have encountered numerous challenges that have made it difficult to ach...

yessine by Associate III
  • 2274 Views
  • 3 replies
  • 3 kudos

FP-AI-PDMWBSOC incorrect inferencing results

I have a STEVAL-PROTEUS device that I collected data with and NanoEdgeAI returned a model that has very high accuracy (almost 100%). In fact, during the validation step on NEAI, the emulator returns very accurate results as well. However, in the depl...

t_mo_0-1724765216981.png
t_mo by Associate
  • 1100 Views
  • 2 replies
  • 0 kudos

Can not add signal from usb (serial)

Hi everyone,I am using version 4.5.0 of Nano Edge AI with the STEVAL-PROTEUS1 sensor kit. I am trying to implement anomaly detection for motor vibration. However, when I attempt to add a signal using USB (serial), I occasionally receive meaningless 1...

Screenshot (86).png

MCU/MPU Selector for AI

In CubeMX I have installed the AI package. After that I go to "Start My project from MCU" then I go to "Middleware" then "Artificial Intelligence" and Enable it.Here, I select whatever model and click Analyze. The button becomes grey, but I don't get...

syalam by Associate
  • 1619 Views
  • 3 replies
  • 0 kudos

sparse model

I have a large PyTorch model that I pruned using unstructured methods to decrease its size. The model size can only decrease if I filter out the zeros and save the model in a sparse format.However, my problem is that ONNX doesn't support the sparse f...

audi by Associate II
  • 2284 Views
  • 1 replies
  • 0 kudos