Skip to main content
Visitor II
May 4, 2024
Question

problem with cube ai

  • May 4, 2024
  • 1 reply
  • 982 views

"I'm facing a challenge with implementing a model on my STM32 board. While the model works flawlessly on some boards, it encounters issues on others. I've verified the hardware compatibility, software configuration, and resource constraints across all boards, but the problem persists. It seems that the model's behavior varies depending on the board, and I'm struggling to identify the root cause. Any insights or suggestions from the community would be greatly appreciated. Thank you!"

 
 
 
 
 
This topic has been closed for replies.

1 reply

fauvarque.daniel
ST Employee
July 17, 2024

It is the same code that runs on the board. We may have some specific optimizations for a specific target but that's it.

The best to verify the compatibility of the board is to run the validation on the target and verify that the "cos" is closed to 1.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.