cancel
Showing results for 
Search instead for 
Did you mean: 

Please check the CUBE AI code.

limjongmin
Associate
This is training data that receives 12 inputs and outputs 1, but strange values appear, so please check and review the code.
 
 
#ifdef __cplusplus
 extern "C" {
#endif
 
/* Includes ------------------------------------------------------------------*/
 
#if defined ( __ICCARM__ )
#define AI_RAM _Pragma("location=\"AI_RAM\"")
#elif defined ( __CC_ARM ) || ( __GNUC__ )
#define AI_RAM __attribute__((section(".AI_RAM")))
#endif
 
/* System headers */
#include <stdint.h>
#include <stdlib.h>
#include <stdio.h>
#include <inttypes.h>
#include <string.h>
 
 
#include "network.h"
#include "network_data.h"
 
#include "app_x-cube-ai.h"
#include "bsp_ai.h"
#include "aiSystemPerformance.h"
#include "ai_datatypes_defines.h"
 
#include <string.h>
#include "ai_datatypes_defines.h"
/* USER CODE BEGIN includes */
/* USER CODE END includes */
 
/* IO buffers ----------------------------------------------------------------*/
 
DEF_DATA_IN
 
DEF_DATA_OUT
/* Activations buffers -------------------------------------------------------*/
AI_ALIGNED(32)
AI_RAM
 
static ai_handle network = AI_HANDLE_NULL;
static uint8_t POOL_0_RAM[AI_NETWORK_DATA_ACTIVATION_1_SIZE];
ai_handle data_activations0[] = {POOL_0_RAM};
/* Entry points --------------------------------------------------------------*/
 
 
void MX_X_CUBE_AI_Init(void)
{
 
ai_error      ai_err;
 
    MX_UARTx_Init();
 
    ai_network_params   ai_params={
              AI_NETWORK_DATA_WEIGHTS(ai_network_data_weights_get()),
              AI_NETWORK_DATA_ACTIVATIONS(data_activations0)
        };
 
    printf("stm32 ai init \r\n");
 
    ai_err   = ai_network_create(&network,AI_NETWORK_DATA_CONFIG);
    if (ai_err.type !=AI_ERROR_NONE)
    {
       printf("ERROR:could not create ai_network_create \r\n");
    }
    if (!ai_network_init(network,&ai_params))
    {
       printf("ERROR:could not create ai_network_init \r\n");
    }
 
   // aiSystemPerformanceInit();
    /* USER CODE BEGIN 5 */
    /* USER CODE END 5 */
}
 
void MX_X_CUBE_AI_Process(void)
{
float   y_val;
 
  ((ai_float *)data_in_1)[0] = (ai_float)25.0f;
  ((ai_float *)data_in_1)[1] = (ai_float)23.0f;
  ((ai_float *)data_in_1)[2] = (ai_float)27.0f;
  ((ai_float *)data_in_1)[3] = (ai_float)30.0f;
  ((ai_float *)data_in_1)[4] = (ai_float)34.0f;
  ((ai_float *)data_in_1)[5] = (ai_float)47.0f;
  ((ai_float *)data_in_1)[6] = (ai_float)68.0f;
  ((ai_float *)data_in_1)[7] = (ai_float)130.0f;
  ((ai_float *)data_in_1)[8] = (ai_float)100.0f;
  ((ai_float *)data_in_1)[9] = (ai_float)10.0f;
  ((ai_float *)data_in_1)[10] = (ai_float)50.0f;
  ((ai_float *)data_in_1)[11] = (ai_float)58.0f;
 
 
 
  ai_network_run(network, &data_ins[0], &data_outs[0]);
 
 
  y_val = ((float *)data_out_1)[0];
 
 
  printf("output: %f\r\n",y_val);
    //aiSystemPerformanceProcess();
    HAL_Delay(1000); /* delay 1s */
    /* USER CODE BEGIN 6 */
    /* USER CODE END 6 */
}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0