cancel
Showing results for 
Search instead for 
Did you mean: 

NanoEdgeAIStudio�?�性能�?�関�?�る�?�?��?��?�?� Inquire about Performance of the NanoEdgeAIStudio.

toyoshima
Associate

詳�?��??調�?��?��?��?�際�?�, �?明�?�点�?��?��?��?��?��?��?��?��?�, �?��?�度�?�連絡致�?��?��?��?�。

以下�?�3点�?��?��?��?��?�回答を�?�願�?�致�?��?��?�。

  1. ​NanoedgeAIStudio�?�必�?メモリ�?��?��??ら�?�?
  2. 時系列データ�?�対応�?��?��?�る�?�?​
  3. 目安�?�良�?��?��?�?一�?�当�?�り�?�価格を�?��?��?��?��?�?​

2月24日(金)�?��?��?��?�回答頂�?��?��?��?�幸�?��?��?�。

�?�忙�?��?��?��?��?�??縮�?��?��?�,�?�回答�?�程よ�?�?��??�?�願�?�致�?��?��?�。​

Excuse me.​

I would like to know more about performance of NanoEdgeAIStudio​.

I would appreciate it if you could tell me three things about it.

  1. What memory do you want to need for operation?
  2. Could I please support the time series data ?
  3. ​How much would it be ?

I would like a response by 2 day later, is that possible?

Looking forward to hearing from you.

1 ACCEPTED SOLUTION

Accepted Solutions
Foued_KH
ST Employee

Hello @滉一 豊嶋​ ,

I recommend you this WIKIs :

AI:NanoEdge AI Studio - stm32mcu

AI:NanoEdge AI Emulator for anomaly detection (AD) - stm32mcu

Also you can have a look : NanoEdge AI Studio V3 Product Overview - YouTube

You need to define limit Flash memory and the max RAM size

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Foued_KH
ST Employee

Hello @滉一 豊嶋​ ,

I recommend you this WIKIs :

AI:NanoEdge AI Studio - stm32mcu

AI:NanoEdge AI Emulator for anomaly detection (AD) - stm32mcu

Also you can have a look : NanoEdge AI Studio V3 Product Overview - YouTube

You need to define limit Flash memory and the max RAM size

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Dear KHALSI​

Thank you very much for your quick reply.

I enjoyed the opportunity to know some information.

​SIncerely,

Toyoshima