2025-02-10 2:01 AM
Hi,
im having issues with NEAI Studio. I was able to craete a project, add signals but when running the benchmark I get an error message that benchmarking was not successfull. In the log I see a lot of this error messages:
optimizer ERROR T20* - An error occurred in neai lib due to Error in qualif, return code: 53
Regards
Max
2025-02-10 2:32 AM
Hello @The_Maxx ,
Can you attach the logs as a zip files, please?
Are you using the 4.6.0? Did you installed this version directly or did you do an update from a previous version?
Have a good day,
Julian
2025-02-10 6:41 AM
2025-02-10 7:39 AM
Hello @The_Maxx ,
Thanks for the information.
This issue means that the search algorithm is looking outside the possible space of possibilities for the parameters of models.
We have already encountered this issue in the past and it was supposed to be fixed. But in our case, it was not really blocking. What do you mean when you say you get an unsuccessful benchmark?
Does the benchmark stop? Do you have anything is the "Validation Step"?
Is it possible for you to share your project? It not, no worries.
Have a good day,
Julian
2025-02-10 2:58 PM
Hello @The_Maxx
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Roger