2025-03-25 5:31 AM
I used the N6 to run the mobilenet_v1_0.25_224_fft_int8.tflite, input is correctly put into the input buffer, memory map activated, NPU RAM enabled, AXICACHE enabled, everything seems to be right, the input I also test the input inside the PC in python, and the model can output things right.
I dot know why, but in some steps it either jumps in to HardFault_Handler (if I directly start the debugging process without any break point)
or runs everything right (using some breakpoints inside the runtime and network.c) but outputs are all Nans
do you have any ideas how I can fix them ?