cancel
Showing results for 
Search instead for 
Did you mean: 

I was using FP-VISION and need to connect another device with Arduino connector

Jerrin_J
Associate

Hi,

I am working on stm32h747i-Disco board, I was in using FP-VISION (person detection) for the ai model to work on my board.

And that's fine, it works well but now i need to connect and esp01 or Pico W with UART or with SPI.

i just modified the code to do so but it did not worked, I just tested my code with another file and the code worked well. so can you clear me whether  the UART or SPI is connectable or not when the FP-VISION is running ?

(i used UART8 or SPI5,And i mainly in UART code when i initialize the uart8 it stops with the menu display which usually comes when started) 

1 REPLY 1
Julian E.
ST Employee

Hello @Jerrin_J,

 

The FP VISION is deprecated (even if it is still written that it is active, changing status on st.com take time because of internal processes...).

I cannot help you with that as the team developing it does not make support anymore.

 

Instead of using FP for AI, the ST Model Zoo was developed. I highly encourage you to take a look at it:

https://github.com/STMicroelectronics/stm32ai-modelzoo 

 

The way it is being made, you should easily be able to replicate what was done in this function pack and even more.

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.