Skip to main content
KSOdin2
Associate III
January 19, 2022
Solved

I have an error code is 23, type is 19, which is AI_ERROR_CODE_INVALID_FORMAT. Is there certain mistakes I could be making?

  • January 19, 2022
  • 1 reply
  • 992 views

I've followed the example on Embedded Inference Client API. However when I run the model I get the error code 23 and type 19 which is the AI_ERROR_CODE_INVALID_FORMAT.

I've checked the type with the following code and both the input and output return 1 for float_stat, this shows that it is a float type

 /* Extract format of the first input tensor (index 0) */

 volatile const ai_buffer *ai_input_1 = &ai_input[0];

 /* Extract format of the tensor */

 fmt_1 = AI_BUFFER_FORMAT(ai_input_1);

 //Extract the float value 1 = float type

 float_stat = AI_BUFFER_FMT_GET_FLOAT(fmt_1);

I've included my code to see if there is something obvious. I have used the API reference that is accessed through CubeIDE but I have found no help. I'm unsure of any other documentation that may help either or examples. I've removed the default code to make it easier to read.

An Onnx model was used which is a sklearn model that has been converted. I was able to upload, analyse, graph and validate successfully. I have set the component set to the application template.

#include "main.h"

#include "string.h"

#include "app_x-cube-ai.h"

#include <stdio.h>

#include "model.h"

#include "model_data.h"

/* Global handle to reference the instantiated C-model */

static ai_handle model = AI_HANDLE_NULL;

/* Global c-array to handle the activations buffer */

AI_ALIGNED(32)

static ai_u8 activations[AI_MODEL_DATA_ACTIVATIONS_SIZE];

/* Array to store the data of the input tensor */

AI_ALIGNED(32)

static ai_float in_data[AI_MODEL_IN_1_SIZE];

/* or static ai_u8 in_data[AI_NETWORK_IN_1_SIZE_BYTES]; */

/* c-array to store the data of the output tensor */

AI_ALIGNED(32)

static ai_float out_data[AI_MODEL_OUT_1_SIZE];

/* static ai_u8 out_data[AI_NETWORK_OUT_1_SIZE_BYTES]; */

/* Array of pointer to manage the model's input/output tensors */

static ai_buffer *ai_input;

static ai_buffer *ai_output;

int aiInit(void) {

 ai_error err;

 /* Create and initialize the c-model */

 const ai_handle acts[] = { activations };

 err = ai_model_create_and_init(&model, acts, NULL);

 if (err.type != AI_ERROR_NONE) {

 while(1){} };

 /* Reteive pointers to the model's input/output tensors */

 ai_input = ai_model_inputs_get(model, NULL);

 //ai_input[0] = 1;

 ai_output = ai_model_outputs_get(model, NULL);

 return 0;

}

volatile ai_error err;

volatile  ai_i32 n_batch;

volatile int float_stat;

volatile ai_buffer_format fmt_1;

volatile int float_stat_out;

volatile ai_buffer_format fmt_1_out;

int aiRun(const void *in_data, void *out_data) {

 /* 1 - Update IO handlers with the data payload */

 ai_input[0].data = AI_HANDLE_PTR(in_data);

 ai_output[0].data = AI_HANDLE_PTR(out_data);

 /* Extract format of the first input tensor (index 0) */

 volatile const ai_buffer *ai_input_1 = &ai_input[0];

 /* Extract format of the tensor */

 fmt_1 = AI_BUFFER_FORMAT(ai_input_1);

 //Extract the float value 1 = float type

 float_stat = AI_BUFFER_FMT_GET_FLOAT(fmt_1);

 /* Extract format of the first output tensor (index 0) */

 volatile const ai_buffer *ai_output_1 = &ai_output[0];

 /* Extract format of the tensor */

 fmt_1_out = AI_BUFFER_FORMAT(ai_output_1);

 //Extract the float value 1 = float type

 float_stat_out = AI_BUFFER_FMT_GET_FLOAT(fmt_1_out);

 /* 2 - Perform the inference */

 n_batch = ai_model_run(model, &ai_input[0], &ai_output[0]);

 if (n_batch != 1) {

   err = ai_model_get_error(model);

   };

 return 0;

  

int main(void)

{

 aiInit();

 volatile float input_buffer_fl[4] = {0.02238, -0.06696, 0.00111 ,-0.12979} ;

 while (1)

 {

 for(int i; i<4; i++){

 in_data[i] = input_buffer_fl[i];

 }

  aiRun(in_data, out_data);

 MX_X_CUBE_AI_Process();

 }

}

    This topic has been closed for replies.
    Best answer by KSOdin2

    Problem solved.

    I was writing this code in main while I had the application template selected. I believe the variable names in both my main and template were the same so was causing clashes. Or I had not set up the input or output correctly. It may be the output as I set it to size 1 when the template set it to size 2. On the template version, it seems there are 2 outputs, one is the class and the other is the value/confidence. This would explain the problem with wrong size (the error code does not inform you whether it is input or output).

    I recommend using the template if you are having issues. The only problem with the template is that I can not set the input and outputs buffers values to float with the code generation. I must do it manually by changing all ai_i8 to ai_float. Then I must change the AI_MODEL_IN/OUT_SIZE_BYTES to AI_MODEL_IN/OUT_SIZE as this will change it to a float size. The only problem with this is that if I regenerated the code it might overwrite and remove my changes.

    If anyone finds a way to have the code generate a float format rather than ai_i8 let me know.

    1 reply

    KSOdin2
    KSOdin2AuthorBest answer
    Associate III
    January 21, 2022

    Problem solved.

    I was writing this code in main while I had the application template selected. I believe the variable names in both my main and template were the same so was causing clashes. Or I had not set up the input or output correctly. It may be the output as I set it to size 1 when the template set it to size 2. On the template version, it seems there are 2 outputs, one is the class and the other is the value/confidence. This would explain the problem with wrong size (the error code does not inform you whether it is input or output).

    I recommend using the template if you are having issues. The only problem with the template is that I can not set the input and outputs buffers values to float with the code generation. I must do it manually by changing all ai_i8 to ai_float. Then I must change the AI_MODEL_IN/OUT_SIZE_BYTES to AI_MODEL_IN/OUT_SIZE as this will change it to a float size. The only problem with this is that if I regenerated the code it might overwrite and remove my changes.

    If anyone finds a way to have the code generate a float format rather than ai_i8 let me know.