cancel
Showing results for 
Search instead for 
Did you mean: 

How NanoEdge AI embeds multiple library models in one code?

szxx
Associate

I would like to ask how NanoEdge AI embeds multiple library models in one code, for example: I compiled a project called "test" in the Keil compiler and I want to create a project similar to an official demo video. Under the same project, there is both an anomaly detection (AD) library for learning and a multi classification (N-Classfial) library for classifying abnormal situations.

Now, I have trained two models for these two libraries, but the problem is that I don't know how to embed these two models into the same project for use. I am using the v5.0.2 version of NanoEdge AI STUDIO.

Can you help me solve this problem? Thank you.

0 REPLIES 0