cancel
Showing results for 
Search instead for 
Did you mean: 

Example reference for ST-Neural-ART accelerator build with MDK-ARM Toolchain

Vishal95
Associate

Could Anyone please help me with the Example application where MDK-ARM toolchain is used to build the application using ST Neural-ART accelerator™. I have STM32N6570-DK evolution kit and I'm trying to develop a prototype for KWS usecase. We have already used the example project provided for STM32CubeIDE with GCC compiler to get started. But, there are no .IOC file is available to modify the example code to develop other use cases.

 

Also wanted to know, what if I build the application that uses ST-Neural-ART accelerator with MDK-ARM would it be able to take advantage of Arm compilor, or such applications can only build with STM32CubeIDE. If it can be build with MDK-ARM, Please provide the example reference so we can finalize the chip for our production.

0 REPLIES 0