Skip to main content
THarn
Associate
July 9, 2019
Question

Error in Validation on target

  • July 9, 2019
  • 1 reply
  • 827 views

Hello,

I flashed my STM32F4-Discovery. If I want to validate on target I get the following error:

"ERROR: no connected board(s) or invalid firmware or the board should be re-started"

I think my error comes up with the firmware, but how can I solve it?

Best regards

Tim

This topic has been closed for replies.

1 reply

Gln
ST Employee
July 17, 2019

Hi Tim,

After building and flashing the "Validation" project onto your STM32F4-Discovery board, are you able to see some output in a serial terminal application (e.g. TeraTerm)?

If not, please check you project is correctly configured with the correct UART pins and correctly programmed.

If yes, you might have another program using the com port instance. Close any opened serial terminal applications.

More information can be found in Section "10.5.1 Error: no connected board, invalid firmware, or board restart needed" of the X-CUBE-AI User Manual (UM2526): https://www.st.com/resource/en/user_manual/dm00570145.pdf

Best regards,

Guillaume