cancel
Showing results for 
Search instead for 
Did you mean: 

Class in the output of the refernece model

pepsi_zero_sugar
Associate II

When I used validation app I could see like 

 notes: - the output of the reference model is used as ground truth/reference value 

        - 10 samples (5 items per sample) 

  acc=100.00%, rmse=0.000000147, mae=0.000000066, l2r=0.000000430, nse=1.000, cos=1.000 

  5 classes (10 samples) 

  --------------------------------- 

  C0        0    .    .    .    . 

  C1        .    0    .    .    . 

  C2        .    .   10    .    . 

  C3        .    .    .    0    . 

  C4        .    .    .    .    0

Now I'm writing a inference code by using template app. 

How can I process output to know what class is the input data?

 

pepsi_zero_sugar_0-1724124147197.png

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
fauvarque.daniel
ST Employee

This document Documentation/embedded_client_stai_api_example.html in the embedded documentation gives you example on how to get the output.

Then the way to process it really depends on your network and the output types (float, int)

Regards

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
fauvarque.daniel
ST Employee

This document Documentation/embedded_client_stai_api_example.html in the embedded documentation gives you example on how to get the output.

Then the way to process it really depends on your network and the output types (float, int)

Regards

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.