2014-11-19 7:24 AM
Hello,
I am trying to make a simple project that for a start can send a single CAN frame.I am using the SPC560B-DIS evb without any CAN board (will connect later on my own converter).I took a CAN sample from other evb and merged it to my project but it doesn't work!Is there any CAN sample that works that I can use?Can I connect a scope to the TX pin and view the data without converter to CAN High and CAN Low?In the example i did not see any initialization to the I/O (Tx and Rx) is that correct?Can I use the external clock on my board for the CAN module?ThanksShachar2014-11-19 8:25 AM
Hello Rosen ,
Do you succeed to take the hand by JTAG USB and PLS? There is an application for motherboard & mini-module SPC560Bxx OS-Less CAN Test Application You can use like starting point these application (importing from Appwizard) SPC560Bxx OS-Less Test Application for Discovery Take the CAN configuration of SPC560Bxx OS-Less CAN Test Application and use these configurations into SPC560Bxx OS-Less Test Application for Discovery WARNING : the io settings are different and the clocks settings are completely different otherwise you should not boot. Anyway , we will update the application repositories in the following weeks especially for discovery boards. yes , it is possible to connect to the TX pin and view the data compare SPC560B6DIS I/O headers with your reference manual. CAN peripheral is started by canStart. for the CAN module , you can use an external clock by settings your low level drivers option. Best regards Erwan ________________ Attachments : 2014-11-19_172054.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qW5u&d=%2Fa%2F0X0000000bo4%2FEnbKO0oN0Q2qgoSvrFzC5hpPT3WMg2w5C4w_Hl7EzPM&asPdf=false2014-11-20 1:25 AM
Hello Erwan,
Thanks for the quick response.I did manage the JTAG USB and PLS, took me a while but it works now.Regarding your suggestion, that is exactly what I did yesterday but no luck with it.question:1. Why isn't there any CAN I/O defined in the example? Shouldn't it be configured in the configuration file just like the Leds and the Push button?2. Is there an option to use C++ compiler during the evaluation period?Thank you,Shachar2014-11-20 5:35 AM
Hello Rosen ,
1) About CAN driver ,
the 8 first mailbox id are dedicated for RX (canReceive) (Input) the 8 next mailbox id are dedicated for TX (canTransmit) (Output) the component GUI (on CAN) is used to enable , disable and configure your CAN Drivers.The test application is to send a CAN Message on a channel with EID 0x1234567
2) We are using a ''gcc powerpc vle'' provided by hightec.
there is no option to use the C++ compiler. it is existing in our plugin : c:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec_1.0.0.201306281422\hightec\bin\ppc-vle-g++.exe you have to create and update your platform component to provide the compilation on c++Best Regards
Erwan
Hello Erwan,
Thanks for the quick response. I did manage the JTAG USB and PLS, took me a while but it works now. Regarding your suggestion, that is exactly what I did yesterday but no luck with it. question: 1. Why isn't there any CAN I/O defined in the example? Shouldn't it be configured in the configuration file just like the Leds and the Push button? 2. Is there an option to use C++ compiler during the evaluation period? Thank you, Shachar2015-01-07 5:10 AM
Hello Rosen
I have the same problem i wrote the code and compile it successfully but no action on Tx CAN Pin is your problem solved ? if you know what is the problem please help me on this thanks Best Regards vanima2015-01-16 6:25 AM
Hello Vanima ,
I have no problem :About the current CAN driver , the 8 first mailbox id are dedicated for RX (canReceive) (Input) (1,2,3,4,5,6,7,8) the 8 next mailbox id are dedicated for TX (canTransmit) (Output) (9,10 ....16) Tx Channel ID 1 means 9 (in lld part) ....and so on ..Next Week, There is will be a improvement on CAN driver on the version 3.4.0#281492 CAN Naming convention : Change the id number of Filter
#286966 The message buffers Tx/Rx Configuration in CAN module
will be dynamic
Best regards Erwan2015-04-02 4:27 AM
2015-04-07 8:22 AM
2015-04-09 3:48 AM
2015-04-29 8:47 AM