cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5Studio does not allow to select receive pin for CANFlex0

Yannek
Associate III

Hello,

I am configuring pin map for SPC560B50L1. I expect to configure pins 14 and 15 as CANFlex0 TX and RX respectively.

Due to manual, pin 15 is the one for CAN-RX for my 64-pin UC:

0690X00000ArxglQAB.png

But this pin has no other option to select than SIUL/GPIO17:

0690X00000ArxgvQAB.png

For another CANbus (CANFlex3) there is an option CAN3RX for the pin 62, so I think it is a bug of SPC5Studio, isn't it? Or am I doing something wrong?

0690X00000ArxhKQAR.png

Best Regards,

Yannek

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

hello ,

It is not a bug.

For PB[1] , CAN0RX is an intrinsec function .. you have to set in Digital Input.

Best Regards

Erwan

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee

hello ,

It is not a bug.

For PB[1] , CAN0RX is an intrinsec function .. you have to set in Digital Input.

Best Regards

Erwan

Thank you, Erwan