2014-11-19 12:41 AM
SPC5STudio 3.3.1 is available !
Dear Users,
The 3.3.1 release is now available on the update site.Minor fixes about :- SPC5Studio CORE : OSAL Component : Error: For input string: in property Number- ISR Code Generation error in OSAL Component- Compatibility issue when adding a component from platform to non-platformWe wish you a happy usage.The SPC5Studio team.2014-12-02 1:47 AM
Dear Mr. Erwan,
I added the URL of the update site in SPC5 Studio and followed the instructions provided in the post:SPC5Studio new update 3.2.0 available
But even after installing all available updates, I still have the 3.0.0 version of the SPC5 Studio. Attached is a screenshot of the ''Install new software'' window. Can you help me identify what the problem is? Thank you in advance, Best Regards, Riadh ________________ Attachments : Capture.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVue&d=%2Fa%2F0X0000000bo2%2FDN83j8P6RNRd1Z1opBqm7Xyds9ohaHW2dVviXcgogSk&asPdf=false2014-12-02 5:07 AM
Hello Riadh ,
Warning , About Dialog is not updated.your ''Installation Details'' should show that the core feature version is 3.3.1 (Button INSTALLATION DETAILS)if the update site shows ''already installed , it means that you are already on 3.3.1 Best Regards Erwan2014-12-02 5:24 AM
It appears the about dialogue is not updated, the installation details gives the right information.
Thank you for your assistance.Best Regards,Riadh