2026-01-19 12:26 AM
Dear community,
I am currently working with the SPC58 E-Line processor placed in the mother daughter evaluation board.
I am using the AEK-MCU-SPC5LNK with OpenOCD. The reference manual for the E-Line is similar o the G-Line. I have only found the SVD file for the G-Line, so I therefore thought, that using this SVD file could work. Sadly the peripherals remain blank and I cannot see any memories.
I would be very happy if someone could tell me, how to get the correct SVD file or what do I have to change to get it running.
Kind regards,
Tassilo
P.s I have used the attached manual, to access the peripherals: How to use the AEK-MCU-SPC5LNK programmer and debugger for SPC5 automotive microcontrollers - User manual