2015-10-14 6:30 AM
Pin wizard was so buggy on SPC564B74L7 I decided to use the standard declaration. On SPC56EL60's RM we can find input mux select config (PSMI) for each input function. On SPC564B74 the RM the PSMI config are placed in another table which makes configuration horrible...
Concerning the pin wizard, it detects error on next opening and worst, it introduce error like declaring many times PORT_A pin 0, 1, 2... Please fix that feature.2015-10-15 8:11 AM
Issue solved on S¨PC5Studio 3.7.0
BR Erwan