cancel
Showing results for 
Search instead for 
Did you mean: 

SPC560D40L1: To drive a 26-Pin 7-segment display LCD from SPC56D-Discovery .

harsh2
Associate II
Posted on May 23, 2016 at 11:17

Hi All

i am driving a 26-Pin(4 COM+22 Segment) LCD display through 

SPC56D-Discovery BOARD Using GPIOs & want to run a counter from 1 to 100 on LCD display.

please advise how it will be possible.

attaching datasheet of LCD.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
harsh2
Associate II
Posted on May 23, 2016 at 14:00

i have displayed the all segments with the help of delay logic & running the lcd at 50hz.

Pls advise if any in-built lcd driver is there in SPC560D40L1 mcu, as i am unable to see in its datasheet.

Regards

Harsh

Erwan YVIN
ST Employee
Posted on May 25, 2016 at 10:27

Hello Harsh ,

There is no built-in driver

Yes , it is possible.

Could you give me your LCD Reference ?

This LCD is supporting I2C ?

We have already implemented some LCD drivers with I2C (sw emulated) to reduce the number of wires

           Best regards

                        Erwan

harsh2
Associate II
Posted on May 30, 2016 at 09:47

Hi Erwan

below is the specs of my LCD:

Specifications:

1. Operating Temperature: -30 to +85 deg C.

2.Storage temperature: -40 to 95 deg C

3.Operating Voltage: 5V

4. LCD Type: TN Positive

5.Connection type: Pin type

6.Clock viewing: 6'o clock

7. Drive condition: 1/4 DUTY, 1/3 BIAS

8.Display type: Trasflective

9.Polarizer colour: Grey

Polarizer: High quality anticlar.

Vibration On cluster: freq: 30-500Hz.

I am attaching its datasheet also.

No, it doesn't support I2C.

Please advise, if i can drive it's display using GPIOs or any other best method.

Awaiting for your kind reply.

Regards

Harsh

________________

Attachments :

LCD_display_-_Electronics.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtbE&d=%2Fa%2F0X0000000aS5%2FX6xBk2_lW04eDgFMta0l76s6S8_jzLTm9EVQUAeHrac&asPdf=false
Erwan YVIN
ST Employee
Posted on May 31, 2016 at 09:37

Hello Harsh ,

There is enough GPIOs to handle a TN Positive LCD. (cf screenshot)

you should create your own driver by creating a new component or new drivers in SPC5Studio.

I am checking in application team if some examples are existing.

Best Regards

Erwan

________________

Attachments :

2016-05-31_093435.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtfG&d=%2Fa%2F0X0000000aVX%2Fkgb80xikGIG84QMQA.8wm6ZtIV0aW28RhppRYYKMFTM&asPdf=false
harsh2
Associate II
Posted on June 13, 2016 at 13:40

Hi Erwan

Please let me know if there are any example codes available for this.

Regards

Harsh