cancel
Showing results for 
Search instead for 
Did you mean: 

SPC560B-DIS Discovery Board

kevin239955_st
Associate II
Posted on October 21, 2014 at 18:35

Can't seem to connect to the SPC560B-DIS via USB or JTAG-USB (SOC5-UDESTK) to the UDE debugger. UDE does not list the device SPC560B54L5. UM1672 User Manual (Table 3) mentions some ''jumper'' states that are in actual fact not jumpers and would require soldering to change configuration.

Can someone help?

#spc5studio
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
12 REPLIES 12
Erwan YVIN
ST Employee
Posted on January 21, 2015 at 17:35

Good news ;)

    Best regards

        Erwan

souha
Associate II
Posted on June 01, 2015 at 17:04

Hello,

We are using the spc560B60L3 100 pin package in adevelopment project. We need to use 4 LINflex interfaces.

In the data sheet, it is mentioned that it supports 4 LINs.Can we use LIN4 and LIN5 or it only supports LIN0 up to LIN3?

Thanks