cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5-UDESTK Tool

SJabl
Associate

Hello,

Im searching for a simple solution to flash several prototypes.

Since our Lauterbach Debugger has been used for HIL testing there is the need for

a 2nd solution.

Recently there are two Questions left:

1. Is it possible to flash also NXP/Freescale 5604 types using the SPC5-UDESTK oder is this locked ? (We have mixed Yield depending on the REV of the PCB)

2. Can I use Trace32 from Lauterbach with the SPC5-UDESTK ?

thx in advance.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Matthias Noack
Associate II

SPC5-UDESTK is usable with STM controllers only.

For a stand alone flash solution with automation capabilities have a look at PLS's website www.pls-mc.com