2019-05-24 04:58 AM
Hello,
Im searching for a simple solution to flash several prototypes.
Since our Lauterbach Debugger has been used for HIL testing there is the need for
a 2nd solution.
Recently there are two Questions left:
1. Is it possible to flash also NXP/Freescale 5604 types using the SPC5-UDESTK oder is this locked ? (We have mixed Yield depending on the REV of the PCB)
2. Can I use Trace32 from Lauterbach with the SPC5-UDESTK ?
thx in advance.
2019-06-27 12:10 AM
SPC5-UDESTK is usable with STM controllers only.
For a stand alone flash solution with automation capabilities have a look at PLS's website www.pls-mc.com