2018-07-11 11:07 AM
Hello all,
I am using SPC570s-Disp eval board and I want to activate the SARADC lld's. I have selected it in the Low Level Drivers Component RLA page, as shown in the screenshot. However, in the MCU wizard tool, it is still shown as inactive (again given in the screenshots). In the code (saradc_lld.h and saradc_lld.c) it seems like the driver enable switches for all the channels (SARADCD12_1, SARADCD12_2 etc.) are undefined.
After trying to build, I get the following error messages
components/spc570sxx_platform_component_rla/lib/rsc/rules.mk:122: recipe for target 'build/obj/main.o' failed
make: *** [build/obj/main.o] Error 1In file included from ./components/spc570sxx_low_level_drivers_component_rla/cfg/spc5_lld_cfg.h:30:0, from ./components/components.h:32, from ./components/components.c:21:./components/spc570sxx_low_level_drivers_component_rla/lib/include/saradc_lld.h:240:2: error: &sharperror 'SARADC driver activated but no SARADC peripheral assigned' &sharperror 'SARADC driver activated but no SARADC peripheral assigned' ^components/spc570sxx_platform_component_rla/lib/rsc/rules.mk:122: recipe for target 'build/obj/components.o' failedmake: *** [build/obj/components.o] Error 1How can I activate the drivers and assign the SARADC peripheral properly?
Thanks in advance.
#saradc_lld2018-07-16 1:54 AM
Hello Yalin ,
Sorry for the late answer,
you should enable Saradc in Low Level drivers
Best regards
Erwan
2018-07-16 2:14 AM
Hello Erwan,
I have enabled the SARADC lld, as shown in capture.png in attachments. It still remains inactive in the MCU wizard.
2018-07-16 3:07 AM
Hello Erwan,
I understand. For now, I have enabled SPC5_SARADC_USE_SARADC12_0 in saradc_lld.h. Thank you.
2018-07-16 5:04 AM
Hello Yalin ,
You are right.
The link is not coded in SPC570sxx component.
i am submitting a ticket to add this link.
you should go directly in the component Low Level drivers
Best regards
Erwan