2024-07-31 8:40 PM
Hi Everyone,
I'm using RX FIFO callback when receiving CAN messages from the ID table in my SPC570S Dev board. According to the reference manual, it only can receive & interrupt the messages from the first 8 IDs (0 to 7) in the table. Is there any way to add more IDs or another way to identify more CAN IDs rather than RX FIFO?
Best regards,
Yohan