2016-02-01 2:01 AM
Hello,
using the SPC56EL70I successfully injected correctable faults in RAM, but after injecting the uncorrectable one with following lines:SPP_MCM.ECR.R=(0x20|0x02); //activate correctable and non-correctable reportingsSPP_MCM.EEGR.R= 0x0220; // inject uncorrectable error*((uint32_t *) 0x40001000) = PATTERN;SPP_MCM.EEGR.R= 0x0000;When I access the location, I get trapped in void osalSysHalt(const char *reason) {osalSysHalt:0x00002AB0: 18 21 06 F0 E_STWU R1,-0x10(R1)0x00002AB4: 00 80 SE_MFLR R00x00002AB6: D5 01 SE_STW R0,0x14(R1)0x00002AB8: D2 31 SE_STW R3,0x8(R1) osalIsrDisable();0x00002ABA: 79 FF FD F7 E_BL 0x000028B0 osal_halt_msg = reason;0x00002ABE: 70 08 E0 00 E_LIS R0,0x40000x00002AC2: C2 71 SE_LWZ R7,0x8(R1)0x00002AC4: 01 06 SE_MR R6,R00x00002AC6: 54 E6 08 B8 E_STW R7,0x8B8(R6) while (1) ;0x00002ACA: E8 00 SE_B 0x00002ACA0x00002ACC: 00 00 SE_ILLEGAL 0x00002ACE: 00 00 SE_ILLEGAL with reason 0x3340 -> clock failure.What am I doing wrong?2016-02-02 8:18 AM