cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any interconnection / relation between port F12 and F13 on SPC560P Disp?

RatheeshT
Associate II

Hi Technical team.

I want to configure both F12 and F13 as input pin.

When i am trying to configure F12 and F13 as input pin in PinMap Editor , it gives error (attached the error screen).

I tried this on sample project "SPC560Pxx_RLA SERIAL Test Application for Discovery".

Hardware used : SPC560P Disp

Please suggest me your ideas to solve this issue

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello Ratheesh ,

Cf reference manual,

It is not possible to configure F12 and F13 with the same function (Ex: GPIO92).

Best regards

Erwan

View solution in original post

5 REPLIES 5
Erwan YVIN
ST Employee

Yes ,

You have tried to configure F[12] and F[13] to the same GPIO

cf Screenshot and reference manual

Best Regards

Erwan

0693W000008GQwAQAW.png

RatheeshT
Associate II

Thanks for your immediate response

From above conversation, My understanding is below,

Port F12 and F13 are not available to configure/use as GPIO pin at the same time in the application

We can use/configure either F12 or F13 only as GPIO at the same time .

is my understanding correct?

or

If my understanding is not correct, Please provide the procedure to configure both F12 and F13 pins as GPIO in SPC5Stusio.

Thanks in advance

RatheeshT
Associate II

Hello Erwan,

Could you please provide your opinion on this.

Erwan YVIN
ST Employee

Hello Ratheesh ,

Cf reference manual,

It is not possible to configure F12 and F13 with the same function (Ex: GPIO92).

Best regards

Erwan

RatheeshT
Associate II

Hello Erwan,

Thanks for your support, I am closing this ticket. It is best