Is it possible to not have a filter when receiving CAN messages?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-10-21 7:52 PM
Is it possible to not have a filter when receiving CAN messages? I want to create a gateway and transfer ALL messages from one CAN bus to another CAN bus. Do I just have to add 1000 messages to my list of allowed messages to ensure everything is accepted?
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-01-19 8:43 AM
Hello ,
Assuming , you have a SPC560D device
You should set your acceptance mask as 0xFFFFFFFF (Cf Below)
Rx Global Mask (RXGMASK)
RXGMASK is used as acceptance mask for all Rx MBs, excluding MBs 14–15, which have
individual mask registers. When the FEN bit in MCR is set (FIFO enabled), the RXGMASK
also applies to all elements of the ID filter table, except elements 6–7, which have individual
masks.
RX14MASK (Rx 14 Mask) and RX15MASK (Rx 15 Mask) have the same structure as the
RXGMASK.
For others devices , please refer to the corresponding RM.
Best regards
Erwan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-01-19 8:43 AM
Hello ,
Assuming , you have a SPC560D device
You should set your acceptance mask as 0xFFFFFFFF (Cf Below)
Rx Global Mask (RXGMASK)
RXGMASK is used as acceptance mask for all Rx MBs, excluding MBs 14–15, which have
individual mask registers. When the FEN bit in MCR is set (FIFO enabled), the RXGMASK
also applies to all elements of the ID filter table, except elements 6–7, which have individual
masks.
RX14MASK (Rx 14 Mask) and RX15MASK (Rx 15 Mask) have the same structure as the
RXGMASK.
For others devices , please refer to the corresponding RM.
Best regards
Erwan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-21 4:13 AM
Hi,
if your CAN controller is using the global mask, just write zero to the global mask value and every configured filter will accept all incoming frames identifiers (standard or extended on the base of filter configuration).
To do this please find the RXGMASK initialization and modify it in order to give zero value.
You should find something like this (maybe in function "can_lld_start" in file "can_lld.c"):
canp->flexcan->RXGMASK.R = 0x0FFFFFFF;
and replace it with --> canp->flexcan->RXGMASK.R = 0x00000000;
Best regards
Domenico